Thank You From Thorlabs Scientific Imaging!

Thank you for installing the host software for our cameras including the ThorImageLS imaging application.

If you wish to run ThorImageLS, you may exit this page and run from the start menu (Press the Start button, then select Thorlabs » Scientific Imaging » ThorImageLS).

If you would like to run third party software applications such as MetaMorph™ , MatLab™ , Micro-Manager you will need to do the following:

  · Ensure that the third party software application of choice is currently installed on your machine

  · Install the necessary plug-in/adapter:

     o  Press Start, then select Thorlabs » Scientific Imaging » Third Party Software Support

     o  When the folder is displayed, double-click on the READ_ME_FIRST html document for more information.

     o  Double-click on the setup program for the software package you want to use.

     o  Follow the instructions

     o  When the installation is complete, you may run your application.