Thorlabs PAX1000 - Change Log Changelog: V1.7 Jul-2025: New features: - Point of view setting. V1.6 Aug-2024 New features: - Support for fast measurement for devices with firmware 1.2.0 - Enable to open many instances of the appplication. (Autoconnect functionality is therefore disabled) - Save ER measurement data as .csv file. V1.5 Jul-2023 New features: - Averaging setting from 1 to 40 samples. V1.4 Apr-2023: New features: - Display stoke parameters in ER measurement view and ER measurement protocol. Bug Fix: - 3D Sphere is not visible with some Intel graphic cards.(Fixed) V1.3 Oct-2022 New features: - Now is possible to navigate through measured points on the poincare sphere. The selected point data will be display on ellipse view. To select the point on the sphere the shift key has to be press. Live data can only be navigated on pause mode. - Circularity parameter is added to the table view. This is a measure how circularly polarised light is. - The firmware update tool is integrated in the PAX1000 software. Bug Fix: - The actual maximal scan rate was not update correctly after the change of the measurement mode.(Fixed) V1.2 Oct-2020 - Default wavelength for PAX1000 metric devices is wrong. (Fixed) V1.1 Dec-2019 - Phase-Difference was displayed in radian and not degree. (Fixed) V1.0 Jun-29-2017 Initial release.