Thorlabs Optical Power Monitor Change Log Since Last Release (V1.1) Version 2.0, published 2019-08-14 Bug Fixes: - For the pyro sensor the NaN values don't increase the samples counter. - The beam size in Y-direction for rectangular beam shape is saved\loaded. - The Graph and Statistics view display recorded time correctly. - Input Filter state setting is displayed for all power meters with this hardware capability. - For the x axis in the graph view the place between the time stamps is now equidistant. - Application checks for updates if this option was actvated. - PM160/PM16 show the correct range New Features: - Added support for power meters that use the NI-Visa USB driver - Added support for PM101 power meters. - Added support for TSP01 and TSP01 rev. B. - Added support for thermopile 4Q sensors - The wavelength value for the PM100USB and PM16 is saved - Each device has now a color indicator in the main view. - Auto Range can be disabled for the PM160/PM16 - A confirmation dialog is opened when the user tries to close the application during logging. Changes: - Statistics\Graph saved files have the same formatting for the numbers as the monitoring file. - Only the selected device can be disconnected from the user interface. Version 1.1, published 2018-09-06 - Adapter type can be selected in the settings.(Adapter) - Trigger Level was added to the settings. (Pyro Sensor) - Bug: Application crash when a device is disconnected. (Fixed) - Change for pyro sensors: Meas functions of the driver internally use the config/fetch commands Version 1.0, published 2018-03-22, initial release